2012-11-28 1:36 PM
I'm trying to upload a ChibiOS demo to the STM32F3 Discovery board. The project builds fine under IAR and appears to connect & program correctly over the onboard ST-LINK. However, when I change the code (i.e. comment out everything, etc) , the board still seems to behave the same so I believe it's not really being programmed.
Is there something I have to do other than Project -> Download & Debug?Both jumpers are on the ST-LINK/Discovery header.2012-11-28 3:47 PM
Well you'll want to make sure you're targeting FLASH and not RAM. That you have not selected a simulated target. And the code is located at the base of FLASH, and not dependent on a Boot Loader.
You could also erase the flash.2012-11-29 7:28 AM
That did it, thanks for the help sir.