2013-04-05 1:12 AM
Hi everybody,
After receiving the board and installing the kit from Keil plus1 hour of struggling with set-up the board was ok :), ran some examples. Ok, excellent, reflashed the ST Link with the new firmware using the ST Link Utility (CRC passed) and started debugging a code of mine, again, no problems. The next day, I had an idea, started my laptop plugged the board and nothing :) I thought it's my mistake or the laptop had problems because it didn't detect the board....Restarted the laptop and the board also, again, nothing, the board wasn't detected by the OS. I tried the same procedure on 4 computers and none detected it....So, the RED LED is blinking and the power led is on...Any ideas ?Thanks,Mihai P2013-04-05 1:22 AM
What OS was this tried on? What code was on board when you shut it down?
2013-04-05 1:25 AM
2013-04-05 3:16 AM
Windows or any other PC - also Windows I might assume? Might I assume Windows 7?
There could be a power problem but I would not know where to search for logs (dmesg) in Windows for that matter...2013-04-05 3:52 AM
The board was test on Win 7 and Win Xp. No results until now. . . .
2013-04-05 3:57 AM
quoting clive1 from another thread: ''If your code is causing a problem pulling BOOT0 High at start up will remove it from being an issue.''
Have you tried this?2013-04-07 4:36 AM