Skip to main content
Tuttle.Darrell
Associate II
September 13, 2017
Question

SPL: NVIC_Init() illogical if not enabling interrupt.

  • September 13, 2017
  • 0 replies
  • 446 views
Posted on September 13, 2017 at 14:09

I just found this out on electronics stackexchange:

If you set the struct member NVIC_IRQChannelCmd = DISABLE, calling NVIC_Init() will do nothing to set the interrupt priority and sub-priority. If you want the interrupt disabled initially and you want to use NVIC_Init(), you will have to enable the interrupt with the struct and then disable it explicitly after calling NVIC_Init() by calling NVIC_DisableIRQ().

Why does NVIC_Init() skip configuring the interrupt priority and sub-priority if the interrupt is to be disabled initially? After seeing the problem on the other forum, I reviewed my own code and found a couple places with the same 'mistake'.

I think it would be dangerous for me to fix NVIC_Init() and recompile the SPL, since the problem would be back with the next download. I think an alternate solution would be to skip using NVIC_Init() and instead use the CMSIS functions: NVIC_EncodePriority() and NVIC_SetPriority() followed by either 

NVIC_DisableIRQ() or  

NVIC_EnableIRQ().

    This topic has been closed for replies.