2012-10-27 7:52 AM
Hi all,
I try too setup an SPI1 com with my STM32F405RG. The datashhet of the component says :SPI Operational Features1. Data is delivered MSB first and LSB last
2. Data is latched on the rising edge of SCLK
3. Data should be transitioned on the falling edge of SCLK
4. The maximum frequency of SCLK is 1MHz
5. SPI read and write operations are completed in 16 or more clock cycles (two or more bytes). The
first byte contains the SPI Address, and the following byte(s) contain(s) the SPI data. The first
bit of the first byte contains the Read/Write bit and indicates the Read (1) or Write (0) operation.
The following 7 bits contain the Register Address.And here is my initialization code (don't work actually) : GPIO_InitTypeDef GPIO_InitStructure; /* Peripheral Clock Enable -------------------------------------------------*/ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); /* Enable GPIO clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 |GPIO_Pin_7; GPIO_Init(GPIOA, &GPIO_InitStructure); #define SPI_INTERRUPTS_ALL (SPI_I2S_IT_TXE | \ SPI_I2S_IT_RXNE | \ SPI_I2S_IT_ERR) SPI_InitTypeDef SPI_InitStructure; SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; /// cad polarity SPI_MODE_0 SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; /// cad phase SPI_MODE_0 SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; // SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; // SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; /* Initializes the SPI communication */ SPI_Init(SPI1, &SPI_InitStructure); SPI_I2S_ITConfig(SPI1, SPI_INTERRUPTS_ALL, DISABLE); SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, DISABLE); /// on autorise les interruptions sur SPI1 RXNE : reception n'est pas vide SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_ERR, DISABLE); /// on autorise les interruptions sur SPI1 RXNE : reception n'est pas vide NVIC_InitTypeDef NVIC_InitStructure; /////// Configure the Priority Group to 1 bit NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); //// Configure the SPI interrupt priority NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); SPI_Cmd(SPI1, ENABLE);If you see anything strange or wrong in my code, I'll be pleased of your help...