cancel
Showing results for 
Search instead for 
Did you mean: 

SPI with DMA Problem

PINI BITON
Associate II
Posted on November 12, 2017 at 19:59

HI

I have stm32f407 evaluation board

I use SPI with DMA to read/send the values

in the 

evaluation board have accelarometer(spi-connect)

this is the data i want to send and i shuold be get acc(x,y,z)

TX_Buffer[0] = 0xA9;//0x80 |0x29;

TX_Buffer[1] = 0xAB;//0x80 |0x2B;

TX_Buffer[2] = 0xAD;//0x80 |0x2D;

i didn't understand how i send and receive data ?

 config DMA and SPI

/////////////////////////////////////

extern volatile uint8_t tempbuff_TX;

extern volatile uint8_t tempbuff_RX;

void CTRLSPI_DMA_init()

{

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);

DMA_InitTypeDef DMA_InitStructure;

DMA_DeInit(DMA2_Stream2);

DMA_DeInit(DMA2_Stream3);

DMA_StructInit(&DMA_InitStructure);

// Configure the Rx part

DMA_InitStructure.DMA_Channel = DMA_Channel_3;

DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(SPI1->DR);

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)tempbuff_RX;

DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

DMA_InitStructure.DMA_BufferSize = NS;

DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;

DMA_InitStructure.DMA_Priority = DMA_Priority_Medium;

DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;

DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

DMA_Init(DMA2_Stream2, &DMA_InitStructure);

DMA_ITConfig(DMA2_Stream2, DMA_IT_TC, ENABLE);

DMA_Cmd(DMA2_Stream2, DISABLE);

//DMA TX.. just modify the relevant parts...

DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(SPI2->DR);

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)tempbuff_TX;

DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral;

DMA_InitStructure.DMA_BufferSize = NS;

DMA_Init(DMA2_Stream3, &DMA_InitStructure);

DMA_ITConfig(DMA2_Stream3, DMA_IT_TC, ENABLE);

DMA_Cmd(DMA2_Stream3, DISABLE);

}

void initSpi(void) {

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);

GPIO_InitTypeDef GPIO_InitStruct;

GPIO_StructInit(&GPIO_InitStruct);

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_DOWN;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_3;

GPIO_Init(GPIOE, &GPIO_InitStruct);

GPIO_SetBits(GPIOE, GPIO_Pin_3);

/*

* configure SPI1 in Mode 0

* CPOL = 0 --> clock is low when idle

* CPHA = 0 --> data is sampled at the first edge

*/

SPI_InitTypeDef SPI_InitStructure;

SPI_I2S_DeInit(SPI1);

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;//| SPI_NSSInternalSoft_Set;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64;// SCLK_freq = APB2_freq / (BaudRatePrescaler + 1)

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

// SPI_InitStructure.SPI_CRCPolynomial = 0;//7;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_Init(SPI1, &SPI_InitStructure);

// SPI_SSOutputCmd(SPI1, ENABLE);

SPI_Cmd(SPI1, ENABLE);

}

#dma #dma-spi #spi
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on November 13, 2017 at 22:08

Is this answered, or was did you mark it so only by mistake?

i didn't understand how i send and receive data ?

By enabling the DMA streams?

JW

Posted on November 15, 2017 at 19:50

can you give me example how to do that?

thanks
Posted on November 15, 2017 at 20:07

Well, I don't use SPL, but you have

DMA_Cmd(DMA2_Stream2, DISABLE);

DMA_Cmd(DMA2_Stream3, DISABLE);

So I'd expect you to have ENABLE somewhere too.

Also, is there no example around in the various EVAL board bundles?

JW