cancel
Showing results for 
Search instead for 
Did you mean: 

SPI hardware Design consideration

mjenabzadeh9
Associate III
Posted on October 01, 2016 at 10:43

Hello 

In my board there are two uc that are connecting through SPI .

Is it necessary to have pullup resistor for spi pins ?

1 REPLY 1
mark239955_stm1
Associate II
Posted on October 02, 2016 at 07:02

It is certainly advisable on at least the Chip Select / Slave Select line or lines.

That said, you can generally configure STM32 I/O lines for internal pullup/pulldown.