Posted on May 17, 2011 at 12:25#define DUMMY_BYTE 0xff 
static unsigned char tx8(unsigned char data) 
{ 
 while ((SPI1->SR & SPI_FLAG_TXE) == (u16)RESET); // Loop while DR register in not emplty 
 SPI1->DR = data; 
 while ((SPI1->SR & SPI_FLAG_RXNE) == (u16)RESET); // Wait to receive a byte 
 return SPI1->DR; 
} 
void spi_tx_8 (unsigned char _data8) 
{ 
 tx8(_data8); 
} 
unsigned char spi_rx_8 (void) 
{ 
 return tx8(DUMMY_BYTE); 
} 
unsigned long spi_rx_32 (void) 
{ 
 unsigned long r; 
 int i; 
 for (i = 0,r = 0; i
 { 
 r |= spi_rx_8(); 
 if (i
 r<<=8; 
 } 
 return r; 
} 
void spi_init (void) 
{ 
 SPI_InitTypeDef SPI_InitStructure; 
 GPIO_InitTypeDef GPIO_InitStructure; 
 /* Enable SPI1 and GPIOA clocks */ 
 RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1 | RCC_APB2Periph_GPIOA, ENABLE); 
 /* Configure SPI1 pins: SCK(PA5), MISO(PA6) and MOSI(PA7) */ 
 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; 
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; 
 GPIO_Init(GPIOA, &GPIO_InitStructure); 
 /* Configure PA.3 as Output push-pull, used as Flash Chip select */ 
 /********* using pc.6 (LED1) 
 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; 
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; 
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; 
 GPIO_Init(GPIOA, &GPIO_InitStructure); 
 */ 
 /* Deselect the FLASH: Chip Select high */ 
 DATAFLASH_CS_HI(); 
 /* SPI1 configuration */ 
 SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; 
 SPI_InitStructure.SPI_Mode = SPI_Mode_Master; 
 SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; 
 SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; 
 SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; 
 SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; 
// SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; 
 SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_16; 
 SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; 
 SPI_InitStructure.SPI_CRCPolynomial = 7; 
 SPI_Init(SPI1, &SPI_InitStructure); 
 /* Enable SPI1 */ 
 SPI_Cmd(SPI1, ENABLE); 
}