2007-11-08 08:58 PM
SPI and Timer
2011-05-17 03:17 AM
Quick questions for my friend on SPI and TImer1,
1) SPI: When the ports are configured as SPI, on the STM it takes up 4 lines: MOSI, MISO, CLK, NSS. (for no dynamic change of master/slave operations) Q,when SPI is enable, can the NSS use as a general GPIO? 2)Timer1, similarly, when some of the ports are configured as timer, say TIM1, which takes up 4 lines TIM CH1-4. Q, if i only use one of them, can i use the other ports as GPIO? Thanks ;-)2011-05-17 03:17 AM