Software interface of STM32F1 with Wifi CC3100 module(simple link driver)
Hi everyone,
Iam trying to integrate the wifi module(CC3100-Simple link)driver files with the stm32f1 microcontroller.
1.After adding the required simplelink driver files with the STM32 code compiled and checked it but getting compile time errror as
253:5: error: unknown type name '_SlCommandHeader_t'
These I tried to solve by
1.Including the required Header files in the respective files.
2.Added the path of the simple link driver files in the stm32 cube ide project properties by
traversing to project->properties->C/C++ general->Paths&symbols
so,none of the above methods worked for me,still facing the same compile time error
please help me to resolve this issue.