2013-03-24 12:27 PM
hi,
i am trying to send data from accelerometer to pc using virtual com port ,but when i open hyper terminal to check if data was sent i found out unsignificant symbols!!!this is the systick handler wich is called when an interruption is generated void SysTick_Handler(void){ uint8_t temp1, temp2 = 0; if (TimingDelay != 0x00) { TimingDelay_Decrement(); } else { Counter ++; if (Counter == 10) { Buffer[0] = 0; Buffer[2] = 0; /* Disable All TIM4 Capture Compare Channels */ TIM_CCxCmd(TIM4, TIM_Channel_1, DISABLE); TIM_CCxCmd(TIM4, TIM_Channel_2, DISABLE); TIM_CCxCmd(TIM4, TIM_Channel_3, DISABLE); TIM_CCxCmd(TIM4, TIM_Channel_4, DISABLE); LIS302DL_Read(Buffer, LIS302DL_OUT_X_ADDR, 6); //routine used to send data via vcp!!! DISCOVERY_EXTI_IRQHandler(); /* Remove the offsets values from data */ Buffer[0] -= XOffset; Buffer[2] -= YOffset; /* Update autoreload and capture compare registers value*/ temp1 = ABS((int8_t)(Buffer[0])); temp2 = ABS((int8_t)(Buffer[2])); TempAcceleration = MAX(temp1, temp2); if(TempAcceleration != 0) { if ((int8_t)Buffer[0] < -2) { /* Enable TIM4 Capture Compare Channel 4 */ TIM_CCxCmd(TIM4, TIM_Channel_4, ENABLE); /* Sets the TIM4 Capture Compare4 Register value */ TIM_SetCompare4(TIM4, TIM_CCR/TempAcceleration); } if ((int8_t)Buffer[0] > 2) { /* Enable TIM4 Capture Compare Channel 2 */ TIM_CCxCmd(TIM4, TIM_Channel_2, ENABLE); /* Sets the TIM4 Capture Compare2 Register value */ TIM_SetCompare2(TIM4, TIM_CCR/TempAcceleration); } if ((int8_t)Buffer[2] > 2) { /* Enable TIM4 Capture Compare Channel 1 */ TIM_CCxCmd(TIM4, TIM_Channel_1, ENABLE); /* Sets the TIM4 Capture Compare1 Register value */ TIM_SetCompare1(TIM4, TIM_CCR/TempAcceleration); } if ((int8_t)Buffer[2] < -2) { /* Enable TIM4 Capture Compare Channel 3 */ TIM_CCxCmd(TIM4, TIM_Channel_3, ENABLE); /* Sets the TIM4 Capture Compare3 Register value */ TIM_SetCompare3(TIM4, TIM_CCR/TempAcceleration); } /* Time base configuration */ TIM_SetAutoreload(TIM4, TIM_ARR/TempAcceleration); /* Read click status register */ LIS302DL_Read(&ClickReg, LIS302DL_CLICK_SRC_REG_ADDR, 1); if(ClickReg == SINGLECLICK_Z) { SingleClickDetect = 0x01; } } Counter = 0x00; } }} and this is the vcp_DataTx function used to send data to USB port :static uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len){ uint32_t i=0; for( i = 0; i < Len; i++ ) { APP_Rx_Buffer[APP_Rx_ptr_in] = (uint8_t) Buf[i]; APP_Rx_ptr_in++; if(APP_Rx_ptr_in == APP_RX_DATA_SIZE) { APP_Rx_ptr_in = 0; } } return USBD_OK;}this function is called into this one : void DISCOVERY_EXTI_IRQHandler(void){ VCP_DataTx (Buffer[0], 1);}thanks in advance .2013-03-24 5:25 PM
I'm not sure I fully understand the point of all that, or what TIM4 is doing, or how, but you're not going to be emitting ASCII data. You look to be trying to send an 8-bit value stored in Buffer[0], which could easily be control characters, or look like other random gibberish in a Hyper Terminal screen. Considered RealTerm printing hex characters?
If you want to get nice signed decimal data out, then you'll need to process the numbers, output the sign, and decode into decimal digits. Also, be cautious about home much you're doing in the SysTick interrupt, I'm not clear of the periodicity of it, or the time it takes to read from the SPI interface here.