cancel
Showing results for 
Search instead for 
Did you mean: 

Selecting right capacitor for oscillator pin used in rtc

aamirali641989
Associate II
Posted on November 29, 2013 at 09:46

I am using rtc & have 32.768Khz cyrstal oscillator (not resonator). I don't have its datasheet. Neither any marking on oscillator.

I have checked AN2867 for capacitor selection i.e CL1 & CL2. But I didn't have datasheet of oscillator. What should be recommended value of capacitor to be used. Currently I am using 10pF. I don't see any problem right now. But I am not sure whether its right?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 29, 2013 at 10:16

But I am not sure whether its right?

May be you could characterize the random crystal, then you'd at least have some data points to actually pluck a value out of thin air? Not even sure which STM32 part you have here, the STM32F405/407 is a lot more sensitive to the characteristics of the circuit. Problems would exhibit as a failure to start, taking a long time to start, or not oscillating in a stable fashion. Sticking a scope probe on the board would typically have a dramatic effect to the circuit.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..