cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO and SD fat access example?

natblist
Associate
Posted on February 09, 2012 at 01:06

Hi Chaps,

Going slowly mad trying to get Chan Fat working with the sdio libs on a stm32f4.

I'm using the most recent (1.0.0) library for the F4, and the low level access demo within that library builds and (at least appears to ) work OK. 

I've spent many, many hours attempting to patch in 0.9 version of fatfs from chan (thks chan, you're a hero) - but I can't get it to work.

If possible, I'd really really appreciate a demo project/source (or direction to - though I've scoured the web and can't find anything that works!)

I'll post separately about the current problems I'm having with the my current build, but a working example would sort it.

Many thanks,

nat.

#hse-sdio-stm32 #stm32-fat-chanfat-fatfs-sdio #sdcard-stm32f4-sdio-fatfs #sdcard-stm32f4-sdio-fatfs
This discussion is locked. Please start a new topic to ask your question.
84 REPLIES 84
Posted on October 22, 2012 at 16:41

Sorry to butt in, Clive1 have you got any other stm32f4discovery projects available we could have a look at? id love to have a play with some of them :)

It's not my platform of choice, but I have ported the USB MSC and VCP examples, as well as FreeRTOS. There are a bunch of USART and servo/pwm examples I've posted here.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aambreen
Associate II
Posted on October 24, 2012 at 09:03

@Clive

I have run your project.

f_mount is returning 0 ( FR_OK)

f_open is returning 1 (FR_DISK_ERROR)

I debugged f_open() function and i have analyzed that in f_open() the call to check_mounted() function is returning 1 (FR_DISK_ERROR)

Inside check_mounted() function vol is assigned 0 and then it skips the part under the comment //Check if the file system object is valid or not. Then the control goes to the part written under the comment //the following code attempts to mount the volume

In this section disk_initialize() function is called and this function is returning 0(disk initialized successfully)

After disk_initialization() function disk_ioctl() function is returning 1 (FR_DISK_ERROR).

aambreen
Associate II
Posted on October 24, 2012 at 10:51

disk_ioctl() function isn't returning any value.I checked the return value on UART but it is not displaying any value.

Posted on October 24, 2012 at 17:12

disk_ioctl() returns RES_OK

You might want to confirm you can do the sector reads (via disk_read(), or equivalent), and verify you can read from the card. If that doesn't work independently, then FatFs will have bigger issues.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aambreen
Associate II
Posted on October 25, 2012 at 07:32

Ok i will get back to you after verifying disk_read() function........i checked f_unlink() function too but it isn't working.....I had been banging my head to figure out the problem since last week :(

aambreen
Associate II
Posted on October 25, 2012 at 08:18

disk_read() function is also returning 1 (not OK) ...... Can you give me code for direct disk_read() call?

Posted on October 25, 2012 at 17:38

unsigned char Buffer[512];

disk_read(0, Buffer, 0, 1);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aambreen
Associate II
Posted on October 31, 2012 at 11:18

@Clive

disk_read() is now functional i have made certain changes in the code and made it working...I have used SD_ReadSingleBlock() to check if this function can read sectors or not

Now tell me the next step?

I want to know the steps that are being followed while implementing FATFS as i don't know the A B C of FATFS....I really want to make my concepts clear as to how this library works and what are the steps that we must follow to implement this file system.

aambreen
Associate II
Posted on October 31, 2012 at 11:22

My ultimate goal is to store an image on SD Card....i would really appreciate if you give me some guideline on this as well

Posted on October 31, 2012 at 15:26

I'm not sure I want to be dragged into your project/work this deep, I think you can read the FatFs documentation/website and source as easily as I can. If you need to understand how it works you'll need to study it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..