cancel
Showing results for 
Search instead for 
Did you mean: 

Schematic to Interface ARM and STM32

harshana_n
Associate II
Posted on May 07, 2011 at 18:42

Goodday !!!

I heard from someone i can use CN3 and program a STM32 using Discovery Evaluation board on a PCB board..

has anyone one has the proper schematic to work this

1 REPLY 1
Posted on May 08, 2011 at 03:04

CN3 breaks the connection to the user programmable STM32 so you connect another board to CN2, the SWD connector. You remove both jumpers, see pg 11 of the user manual.

There are only 4 pins on CN2, and two of those are power. The other two are TCK/SWCLK and TMS/SWDIO, you can see these, and how they would connect to an STM32, by reviewing the VL Discovery schematic. Is this something you have looked at?

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/CD00267113.pdf

Realistically you'd probably want to have a reset too. There are some better JTAG/SWD solutions out there.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..