2009-04-30 7:45 AM
RTC alarm is not accurate
2011-05-17 4:10 AM
Hello all,
I am having some issues with my RTC alarm, Im using the stm32f103 dev kit from iar. I am trying to wake the MCU every second from stop mode with an rtc alarm i have succesfully set the interrupt and they unit is going to sleep then waking up but instead of every sencond it wakes up every 2 ! even tough im setting for that ie. /* Wait till RTC Second event occurs */ RTC_ClearFlag(RTC_FLAG_SEC); while(RTC_GetFlagStatus(RTC_FLAG_SEC) == RESET); RTC_WaitForLastTask(); /* Alarm in 1 second */ RTC_SetAlarm(RTC_GetCounter()+1); /* Wait until last write operation on RTC registers has finished */ RTC_WaitForLastTask(); PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFE); Time_Show(); /* Configures system clock after wake-up from STOP: enable HSE, PLL and select PLL as system clock source (HSE and PLL are disabled in STOP mode) */ SYSCLKConfig_STOP(); it funny because if i use the rtc sec interrupt instead of the alarm i get anice second interrupt but not from the alarm interrupt furthermore i have this debug string shooting to teraterm that tell me what the time is ************ Reset ************ Time Show Time: 24:00:02 Time Show Time: 24:00:04 Time Show Time: 24:00:06 Time Show Time: 24:00:08 Time Show Time: 24:00:10 I am setting the time to be 24:00:00 but as you can see 2 seconds after is when the micro gets woken this tells me that the actual rtc is running fine but for some reason the alarm is screwed up somehow. I am running the micro at 8 mGz HSE and the rtc from the 32 khz LSE here is the RCC config for APB1 and APB2 /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* PCLK2 = HCLK */ RCC_PCLK2Config(RCC_HCLK_Div1); /* PCLK1 = HCLK/2 */ RCC_PCLK1Config(RCC_HCLK_Div2); any ideas guys ??? thank you