cancel
Showing results for 
Search instead for 
Did you mean: 

RSA sign

arunease
Associate II
Posted on April 22, 2016 at 11:59

Hi 

i have a problem with RSA signing. when i use RSA_PKCS1v15_Verify  function from ST library, i get a error of rsa Invalid Key.

is there any function that i can create a modulus?.. 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
slimen
Senior
Posted on April 22, 2016 at 13:46

Hi emb_begin,

Check if your RSA private key structure and parameters are valid.

You can refer to the ''

http://www2.st.com/content/ccc/resource/technical/document/user_manual/group0/f9/6e/f2/a2/b4/ec/49/c0/DM00215061/files/DM00215061.pdf/jcr:content/translations/en.DM00215061.pdf

'' it may be helpful for you.

Regards

SURLEAU.Frederic
Associate III
Posted on March 20, 2018 at 17:02

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6sv&d=%2Fa%2F0X0000000bxI%2FzopxKkXtag2z3FahCMTqEGGQP5_02vK0_5gZ9HcPJk0&asPdf=false
Posted on March 22, 2018 at 09:34

Ok, I found my bug.

Openssl add an extra 0x00 in front of modulux and exponent to make them positive integers.

With

uint8_t privateExponent[] = {
 0xd9, 0x1c, 0xec, 0xb7, 0x5d, 0x79, 0x52, 0xe2, 0x44, 0xd6, 0x6d, 0xa1, 0x92, 0x1a,
0xf0, 0x9d, 0xb3, 0x32, 0x98, 0x89, 0x53, 0x76, 0xbc, 0xac, 0xb3, 0x24, 0x1d, 0xc3, 0xda,
0x55, 0xe0, 0x42, 0xe2, 0x03, 0xc6, 0x4a, 0x2a, 0x29, 0xb2, 0x67, 0xdf, 0x82, 0x8d, 0xfb,
0x8d, 0x05, 0x95, 0xe4, 0x37, 0x9e, 0x0a, 0x02, 0x20, 0x06, 0xff, 0xae, 0x14, 0xa4, 0xe0,
0xbf, 0x35, 0x58, 0x4e, 0xc4, 0x4b, 0x92, 0x13, 0x02, 0xcd, 0x9a, 0xad, 0xa7, 0xf1, 0xec,
0xd5, 0x5b, 0xbf, 0xb8, 0x7c, 0x26, 0x50, 0x7d, 0x70, 0x30, 0x16, 0x6a, 0x18, 0xda, 0x79,
0xe8, 0x86, 0xdb, 0x93, 0x4e, 0x53, 0x34, 0x1a, 0x67, 0x35, 0xae, 0xe0, 0xb8, 0xc5, 0xe6,
0x34, 0x7b, 0x59, 0x62, 0x97, 0xb2, 0x6d, 0x38, 0x33, 0xab, 0xf4, 0xde, 0x4b, 0xc6, 0x88,
0x68, 0xaf, 0x61, 0x30, 0x94, 0x72, 0xa1, 0x2f, 0xc1 };
uint8_t modulus[] = {
 0xda, 0x26, 0xca, 0xf4, 0xd9, 0xa5, 0x17, 0xeb, 0xa7, 0x00, 0x94, 0x2c, 0x01, 0x31,
0xf6, 0x6a, 0xff, 0xcd, 0x0d, 0xd7, 0xbd, 0x16, 0xc6, 0xce, 0xf5, 0x3c, 0xbd, 0xb2, 0x6b,
0xda, 0xc1, 0x59, 0xa6, 0x2f, 0x8c, 0x11, 0x19, 0x39, 0x81, 0x6d, 0xce, 0x50, 0x10, 0xc2,
0x77, 0x40, 0x01, 0xab, 0xd5, 0x42, 0x55, 0x35, 0xae, 0x3f, 0xcf, 0x39, 0xd3, 0x92, 0xfc,
0xf5, 0x64, 0x34, 0x3f, 0x97, 0xb2, 0x89, 0x91, 0xea, 0xf2, 0x9a, 0x8f, 0x80, 0x33, 0x1c,
0x13, 0x48, 0x14, 0xa7, 0xc8, 0x9e, 0x79, 0x98, 0xa2, 0x22, 0xdc, 0xe1, 0xb0, 0x2a, 0x56,
0xa3, 0xe0, 0xd3, 0xd4, 0x26, 0xd2, 0x25, 0xab, 0x54, 0x8a, 0x7a, 0x00, 0x8c, 0x26, 0x93,
0x55, 0x0d, 0xae, 0x67, 0xa2, 0x13, 0x93, 0x0d, 0xde, 0xae, 0x7c, 0x48, 0xc0, 0xc7, 0x79,
0x44, 0x71, 0xfa, 0x7f, 0x58, 0x76, 0x0c, 0xea, 0x81 };

Everything works good.