cancel
Showing results for 
Search instead for 
Did you mean: 

RM0433: What is "Hold boot"?

Uwe Bonnes
Chief

RM0433 Rev 5 in chapter 7.1. talks about "Hold boot function".

The reference manual dose not come up with some explanation later.

Please explain.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi Uwe,

Hold boot isn't supported in RCC embedded in STM32H743/STM32H753/STM32H750 devices. This is an error and has to be removed from the reference manual.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Amel NASRI
ST Employee

Hi Uwe,

Hold boot isn't supported in RCC embedded in STM32H743/STM32H753/STM32H750 devices. This is an error and has to be removed from the reference manual.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.