cancel
Showing results for 
Search instead for 
Did you mean: 

RM0091 errors (TIM15/16/17 section); 32F0xx reference manual

fenugrec
Associate II
Posted on June 02, 2015 at 02:32

Hi,

be warned - RM0091, as of rev. 7 (oct. 2014), has a few errors in section 19 ''General-purpose timers (TIM15/16/17) : it seems some sections were copy-pasted from another timer. Those timers *DO NOT* have a downcounting mode.

* 19.4.1 claims ''counter can count up, down or both up and down''  - nope !

* p.484 : in the note below the figure :''Downcounting configuration [...] when DIR bit in TIMx_CR1 is high.''  nope ! There's no DIR bit in TIM{15,16,17}_CR1

* 19.4.13 One pulse mode: ''- in downcounting: CNT > CCRx''  -> misleading

Fortunately I didn't need to change my design a lot because of this, but others may not be so lucky !

#rm0091
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0