2009-07-14 5:18 AM
Ride7 Interrupts work in Flash but not RAM
2011-05-17 4:17 AM
Hi,
I'm compiling a Timer interrupt example using Ride7 and downloading using RLink. When I select Flash I can happily get my timer interrupt and put a breakpoint on. However if I switch to RAM and change the settings on my STM3210E-EVAL board to SRAM - it compiles and downloads, but I don't get any interrupts. Any ideas what I'm doing wrong? Dex2011-05-17 4:17 AM
Please any information will be helpful. I'm using the latest versions - downloaded 2 days ago. Does anyone know of problems with the default linker script? Is it because I'm using the standard version and need to upgrade to PRO?