2017-07-02 10:29 AM
Hello, I'm using stm32f407vgt6 MCU in a control system and I'm facing a strange problem in the reset circuit, when I power on the system it doesn't start until I put a short circuit wire manually between reset pin and GND and then remove this wire so system can start properly. system's external reset circuit consists of pulldown 0.1uF capacitor and pullup 10KOhm resistor. I have tried to replace the 10KOhm resistor with 100KOhm but nothing changed. I also replaced the 0.1uF capacitor with 1uF and also nothing changed. Could someone help me to find out what may cause this problem and why I need to connect the reset pin to ground for just a second in order for the system to start?
Thanks so much in advance
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-07-02 12:22 PM
What else in your system connects to NRESET, or is dependent on the power supply coming up?
On a scope or analyzer how wide is the reset pulse as built? Can you plot that against the supplies in the system?
What does the part do when it starts? Does it run at all? Does it bring up other clocks, or try to interact with external parts?
Are the capacitors and voltages at VCAP correct?
Consider an external POR circuit thresholding your highest supply, using a MCP120 or similar part, holding the NRST low for several hundred milliseconds.
2017-07-02 5:05 PM
There is only a track connecting the NRESET pin with SWD circuit so I can use it when re-flashing the firmware and by the way when downloading a new code, it starts working properly but when I restart the system by turning power off and then turning it on again it doesn't work and I must connect the reset pin to GND for a second in order for the system to start. As I described the NRST is connected to pulldown capacitor which is connected to system common ground in addition to a pullup resistor which is also connected to system common VDD (3v common with MCU VDD pins).
I will try to plot the reset and power signals on an oscilloscope but I don't think it will be easy to get the transient response of the system.
Voltages on VCAP are 1.26v so I think they are correct.
I didn't try a POR circuit before, could you describe it in more details?
2017-07-02 6:03 PM
The MCP120 has 3 pins, VCC, GND and RESET output, pull a datasheet.
2017-07-02 11:04 PM
Check pins BOOT0 and BOOT1. Maybe they are floating after a POR and the bootloader gets started?
2017-07-03 8:49 PM
I connected BOOT0 directly to GND and according to datasheet when BOOT0 is connected to GNG BOOT1 is don't care so I let it floating, do I need to connect BOOT1 to GND also?
2017-07-03 8:49 PM
I will try using MCP120 with threshold of 3v
2017-07-03 9:00 PM
But what I am finding strange is that this problem happens in some samples of the system and some other work properly without facing any issues, I talking about the same system design. so why?
and I built many different designs with the same reset circuit and it's the first time to face such a problem!
2017-07-04 1:04 AM
IMHO it should be OK this way, as long as you don't plan to start into the bootloader.
Have a look at
https://community.st.com/0D50X00009XkYeESAV
Seems to be the same problem.
I wonder about the pull up resistor on NRST because usually there is an internal permanent pull up allready connected.
2017-07-04 2:12 PM
ST uses a pullup 100KOhm resistor also with STM32F4-Discovery board.