cancel
Showing results for 
Search instead for 
Did you mean: 

Reprogramming the STM32F107 via Ethernet?

Terje Bøhler
Associate II
Posted on May 11, 2017 at 12:31

Hi. 

We use STM32F107 and our customer now wants to include the feature of reprogramming (SW updates) the MCU via Ethernet? How can this be achieved? If 'not possible' with this MCU, are there any other STM32-family MCU that has this feature included?

Best Regards

Terje B�hler

#reprogramming-the-stm32f107-via-ethernet?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 11, 2017 at 13:39

You'd have to completely code the solution, having some place to store the intermediate image would be helpful.

Review the ETH IAP examples for the F1 and other STM32 platforms.

http://www.st.com/content/ccc/resource/technical/document/user_manual/79/6e/5f/d4/5c/25/43/96/DM00103145.pdf/files/DM00103145.pdf/jcr:content/translations/en.DM00103145.pdf

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..