2018-10-16 5:01 AM
Hi..... i am a masters student from india. I have developed a code for RGBW now i want to include strobe effect for that i have give a hal_delay it is working fine now i want to change the PWM of RGBW when it is in strobe effect both has to work simultaneously but it is getting hanged i think this is due to Hal_delay i think this problem will be reduced if i give timer delay or i want to do something if it will solved with timer how to give timer delay in STM Controller.. I am using STM32F407VG controller.. Can someone help me out in this....... Thanks in Advance
2018-10-16 5:51 AM
The HAL_Delay is rather course you could use a 32-bit timer like TIM2 or TIM5 to count microseconds or faster, and delta the TIM->CNT as it advances or use the cores DWT_CYCCNT
The HAL method is also dependent on a interrupt so can be a problem if interrupt priorities are wrong and used in callback routines.
2018-10-26 8:57 PM
I am giving interrupt priority to 0. could you please give me a sample code for better understanding
2018-10-26 8:57 PM
i think timer handler will work out but iam didn't understand how to give it
2018-10-26 11:28 PM
first you would have to initialise the timer... are you using the cube ?
void start_Timer4(void) {
HAL_TIMEx_OCN_Start(&htim4,TIM_CHANNEL_1);
HAL_TIM_Base_Start(&htim4);
}
2018-10-26 11:50 PM
void resetTim2ChannelCounter(TIM_HandleTypeDef *htim, uint32_t channel) {
uint32_t tmp;
tmp = htim->Instance->CNT;
htim->Instance->CCR1 = tmp;
htim->Instance->SR = ! TIM_SR_CC1IF; // clear the flag
}void waitTim2ChannelComplete(TIM_HandleTypeDef *htim) {
uint32_t tmp;
tmp = 0;
while( ! tmp ){
checkBackgroundServices(); // OS services
tmp = htim->Instance->SR & TIM_SR_CC1IF;
}
htim->Instance->SR = ! TIM_SR_CC1IF; // clear the flag
}
2018-10-27 12:05 AM
void MX_TIM5_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;
htim5.Instance = TIM5;
htim5.Init.Prescaler = 84;
htim5.Init.CounterMode = TIM_COUNTERMODE_UP;
htim5.Init.Period = 99; //interrupt in 100 micro sec
// htim5.Init.Period = 50; //interrupt in 50 micro sec
htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
if (HAL_TIM_Base_Init(&htim5) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim5, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim5, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{
if(tim_baseHandle->Instance==TIM5)
{
/* USER CODE BEGIN TIM5_MspInit 0 */
/* USER CODE END TIM5_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM5_CLK_ENABLE();
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(TIM5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM5_IRQn);
/* USER CODE BEGIN TIM5_MspInit 1 */
/* USER CODE END TIM5_MspInit 1 */
}
}
void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle)
{
if(tim_baseHandle->Instance==TIM5)
{
/* USER CODE BEGIN TIM5_MspDeInit 0 */
/* USER CODE END TIM5_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_TIM5_CLK_DISABLE();
/* Peripheral interrupt Deinit*/
HAL_NVIC_DisableIRQ(TIM5_IRQn);
}
/* USER CODE BEGIN TIM5_MspDeInit 1 */
/* USER CODE END TIM5_MspDeInit 1 */
}
void start_Timer4(void) {
HAL_TIMEx_OCN_Start(&htim5,TIM_CHANNEL_1);
HAL_TIM_Base_Start(&htim5);
}
void resetTim5ChannelCounter(TIM_HandleTypeDef *htim, uint32_t channel) {
uint32_t tmp;
tmp = htim5->Instance->CNT;
htim5->Instance->CCR1 = tmp;
htim5->Instance->SR = ! TIM_SR_CC1IF; // clear the flag
}
void waitTim2ChannelComplete(TIM_HandleTypeDef *htim) {
uint32_t tmp;
tmp = 0;
while( ! tmp ){
checkBackgroundServices(); // OS services
tmp = htim->Instance->SR & TIM_SR_CC1IF;
}
htim->Instance->SR = ! TIM_SR_CC1IF; // clear the flag
}
SetPWM(x,dutycycle);
SetPWM(y,dutycycle);
SetPWM(z,dutycycle);
start_Timer5(void);
SetPWM(x,0);
SetPWM(y,0);
SetPWM(z,0);
start_Timer5(void);
is this is what you are asking me to do or some thing else... if any mistake just correct me
2018-10-27 1:11 AM
at some stage you have started your timer...
start_Timer5();
while(1){ ....... }can you add these functions ?
extern "C" void wait_us(int uS) {
resetTimChanneluSCounter(&htim5, 1, uS);
waitTimChannelComplete(&htim5, 1);
}
void resetTimChanneluSCounter(TIM_HandleTypeDef *htim, uint32_t channel, int16_t uS) { // tuned to F767
uint32_t uS_Counts;
if (uS < 8)
uS_Counts = ((int32_t) 13480 *8) / 1000;
else
uS_Counts = ((int32_t) 13480 *(uS-4)) / 1000;
switch (channel) { // used to have &=
case 1: {
htim->Instance->CCR1 = htim->Instance->CNT + uS_Counts;
htim->Instance->SR = !TIM_SR_CC1IF; // clear the flag
break;
}
case 2: {
htim->Instance->CCR2 = htim->Instance->CNT + uS_Counts;
htim->Instance->SR = !TIM_SR_CC2IF; // clear the flag
break;
}
case 3: {
htim->Instance->CCR3 = htim->Instance->CNT + uS_Counts;
htim->Instance->SR = !TIM_SR_CC3IF; // clear the flag
break;
}
case 4: {
htim->Instance->CCR4 = htim->Instance->CNT + uS_Counts;
htim->Instance->SR = !TIM_SR_CC4IF; // clear the flag
break;
}
}
}
void waitTimChannelComplete(TIM_HandleTypeDef *htim, uint32_t channel) {
uint32_t tmp;
tmp = 0;
while( ! tmp ){
checkBackgroundServices(); // OS services
switch (channel){
case 1:
tmp = htim->Instance->SR & TIM_SR_CC1IF;
break;
case 2:
tmp = htim->Instance->SR & TIM_SR_CC2IF;
break;
case 3:
tmp = htim->Instance->SR & TIM_SR_CC3IF;
break;
case 4:
tmp = htim->Instance->SR & TIM_SR_CC4IF;
break;
}
}
switch (channel){ // used to have &=
case 1:{
htim->Instance->SR = ! TIM_SR_CC1IF; // clear the flag
break;
}
case 2:{
htim->Instance->SR = ! TIM_SR_CC2IF; // clear the flag
break;
}
case 3:{
htim->Instance->SR = ! TIM_SR_CC3IF; // clear the flag
break;
}
case 4:{
htim->Instance->SR = ! TIM_SR_CC4IF; // clear the flag
break;
}
}
}
//******************
start_Timer5();
while(1){ ....... }
in your code:
SetPWM(x,dutycycle);
SetPWM(y,dutycycle);
SetPWM(z,dutycycle);
wait_us(10); // blocking code
SetPWM(x,dutycycle);
SetPWM(y,dutycycle);
SetPWM(z,dutycycle);
// non blocking code:
if ( htim->Instance->SR & TIM_SR_CC1IF){ process next PWM }
2018-10-27 1:42 AM
is really CCR1,2,3,4 are required i think ccr1 is enough.... ok i'll try this method and get back to you...
Thank You :)
2018-10-27 2:01 AM
checkBackgroundServices();?
What the above line indicates