2016-12-08 06:35 AM
about
https://community.st.com/0D50X00009XkeG3SAJ
OK for the idea, a small rework to do on the board in this case.
1- i need to disable the pin 13 mangement in the application (BSP_LED) in stm32f746g_discovery.c file in the demonstration project of the board.
what is the default state of the pins if not initialize, please ?
2- Create a new configuration for the spi2 (using for example stm32 cube) with d13,d12,d11 clk, mosi, miso pins.
the base of the configuration that can be found on the projet in the stm32f4x_nucleo.c file
And add a new entry in the stm32_blue_nrg_ble.h file and complete stm32f746g_discovery file.
i didn't find the ico extension file wih the démonstrations to modify the configuration.
Is there a possibility to reverse the ioc file ?
3- create a new entry in the stm32bluenrg_ble.h adding support for this board.
i hope that i'll not lost functionnality about pin affected to spi2 : the goal is to keep all current demo and add ble scanner for example.
Your advice ?
null2016-12-09 09:32 AM
Hi Christophe,
from which source project did you start for the DISCO-F746NG board? Is it the demo code included in the STM32CubeF7 package? That would help me understand what is the best course of action in your case. Which IDE are you using for building?
What kind of project are you working on? Are you planning to build a product out of it or is it for demo purposes?
As for the .ioc configuration file, it is not available yet for the BLE examples included in the X-CUBE-BLE1 software expansion package, but I'll build one for you as soon as possible. Meanwhile, besides creating an entry for your Discovery board in the stm32_bluenrg_ble.h file, you should also create a new file in the BSP directory for the Discovery. As a starting point you could use the
Drivers\BSP\STM32F4xx-Nucleo\stm32f4xx_nucleo_bluenrg.h file that is configured for NUCLEO-F401RE.
Best regards,
Antonio
2016-12-09 12:49 PM
Hi Antonio,
i found a case
http://www.iwasz.pl/uncategorized/bluenrg-stm32f7-disco-tests/
where is a first configuration.i propose you in a first step to realize the configuration of the spi 2 (with screenshot) and synchronize with you.
it's a good challenge to learn and i think usefull to your package so follow me ;->>
i'll begin with the pin configuration.
2016-12-09 01:46 PM
well ... using stm32cubemx we obtain :
and the device configuration (limited spedd to ensure to have a compatible speed):
we obtain spi initialisation
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 7; hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;and spi pin setup :
and pins configurations:
GPIO_InitStruct.Pin = ARDUINO_SCK_D13_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(ARDUINO_SCK_D13_GPIO_Port, &GPIO_InitStruct);GPIO_InitStruct.Pin = ARDUINO_MISO_D12_Pin|ARDUINO_MOSI_PWM_D11_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);enabling interrupt:
2016-12-09 02:59 PM
Arduino D7 (Reset pin) -> PI3
/*Configure GPIO pin : ARDUINO_D7_Pin */
GPIO_InitStruct.Pin = ARDUINO_D7_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(ARDUINO_D7_GPIO_Port, &GPIO_InitStruct);Arduino A0 (Irq) -> PA0
need to reconfigure the interrupt to suport irq
/*Configure GPIO pin : bluenrgirq_Pin */
GPIO_InitStruct.Pin = bluenrgirq_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_PULLDOWN; HAL_GPIO_Init(bluenrgirq_GPIO_Port, &GPIO_InitStruct);Arduino A1 (csn) -> PF10
/*Configure GPIO pin : CSN_Pin */
GPIO_InitStruct.Pin = CSN_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(CSN_GPIO_Port, &GPIO_InitStruct);and Interrupt 1 and 2 screenshot configuration
Arduino D3 (inital clock) to disable on the board or cut the pin on the shield to limit contact -> PB4 to ensure disabled
Adruino D13 to connect to Arduino D3 -> remove the led management in the original project.
2016-12-12 10:19 AM
Hi Christophe,
did you succeed to run the code with this configuration?
Unfortunately I don't have your Discovery board and can't test it myself. As another option, if you need this just for prototyping and not for production, you could also use mbed, where you can program at higher level. You won't be able to squeeze the hardware and get the maximum out of it, but it will be faster to build a demo.
https://developer.mbed.org/platforms/ST-Discovery-F746NG/
https://developer.mbed.org/components/X-NUCLEO-IDB04A1/
If you stick to STM32Cube of course, you will get much more control on the hardware configuration.
Hope that helps,
Antonio
2016-12-13 05:42 AM
i agree with you but i began a training (graphical tutorials) in paris in stm headquarters.
and i'would ensure to take benefit of this training about you professional tools.
Br,
please check about the request of my other topic ;->