RBUS issue on STM32F407
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 11:40 PM
Hello.
I'm working on a new board with STM32F407 MCU.Currently, there's an issue with Ethernet.After board reset, Ethernet communication is working well.
But after some time (minutes or hours), the Ethernet seems to be blocked.ETH_DMASR_RBUS bit (0x00000080) is set when the communication is not ok.
My code was from STM32CubeMX and the versions are as follows.
STM32CubeMX : Version 4.17.0
FreeRTOS : V8.2.3
So, I have added 'ethernet_watchdog' function in the thread 'ethernetif_input'
after searching the web for this issue.
However, it didn't solve the issue.
From my investigation, I have found
that the thread 'ethernetif_input' is waiting forever for the semaphore (s_xSemaphore) to be released.HAL_ETH_RxCpltCallback is being called continuously by the Ethernet ISR (interrupt service routine).s_xSemaphore
is a binary semaphore.I tried changing the semaphore as a counting one (MAX. 10), but no change.
When I replaced the semaphore with osDelay(1), the Ethernet is working well for a long time.
But it has some performance issue possibly because of the delay in the thread.
Well, I'm not sure if it is an issue with the OS.
Please, let me have any help for my issue.Thank you.
ps) Some code for better understanding.Except
ethernet_watchdog, all the codes are directly from STM32CubeMX.
//Function called directly from ISR...
void HAL_ETH_RxCpltCallback(ETH_HandleTypeDef *heth){osSemaphoreRelease(s_xSemaphore);
}//Ethernet Thread...
void ethernetif_input( void const * argument ){struct pbuf *p;
struct netif *netif = (struct netif *) argument;for( ;; )
{ if (osSemaphoreWait( s_xSemaphore, TIME_WAITING_FOR_INPUT)==osOK) { do { p = low_level_input( netif ); if (p != NULL) { if (netif->input( p, netif) != ERR_OK ) { pbuf_free(p); } } } while(p!=NULL); } ethernet_watchdog(); }}static void ethernet_watchdog(void)
{ /* When Rx Buffer unavailable flag is set: clear it and resume reception */ if ((heth.Instance->DMASR & ETH_DMASR_RBUS) != (uint32_t)RESET) { /* Clear RBUS ETHERNET DMA flag */ heth.Instance->DMASR = ETH_DMASR_RBUS; /* Resume DMA reception */ heth.Instance->DMARPDR = 0; }}// Semaphore and Thread creation...
static void low_level_init(struct netif *netif)
{...
/* create a binary semaphore used for informing ethernetif of frame reception */
osSemaphoreDef(SEM);s_xSemaphore = osSemaphoreCreate(osSemaphore(SEM) , 1 );/* create the task that handles the ETH_MAC */
osThreadDef(EthIf, ethernetif_input, osPriorityRealtime, 0, INTERFACE_THREAD_STACK_SIZE); eth_input_handle = osThreadCreate (osThread(EthIf), netif);...
}
#RBUS#STM32F4#ETHERNET#FreeRTOS#
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-15 2:49 AM
Hi,
I advice you to update CubeMx version to use the latest version 4.21 and STM32CubeF4 V1.16.0 which contains limitations fixes and with upgrade to use FreeRTOS v 9.0.0
Please, keep us informed about your update and progress.
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-15 6:45 AM
First of all, thank you for your answer.
I just upgraded the CubeMX as advised
and tested the Ethernet communication after fixing some minor compilation errors.
But the situation is the same.
The source codes doesn't seem to be quite different between 2 versions.
When the problem happens, DMASR is set as 0x00680484.
RBUS and TBUS are both set.
If I clear RBUS and TBUS from a different thread in this situation,
some Ethernet frames are sent, but immediately RBUS and TBUS are set.
So, traffic is blocked again.
Anyhow, please help me to resolve this issue.
Thank you.