2016-05-07 8:21 PM
Hi all,
I have seen a code where a GPIO pin is configured as output in push-pull mode but the pin is driven by an external circuit to low some times (essentially shorting the top transistor to GND). Is it safe to implement such a circuit? Will the I/O pin remain undamaged? Your comments please? Thank you.PS: I have created a sample schematic for clear understanding of my question.2016-05-08 12:25 AM
If you have access to that external circuit, it would be better to make it as a switch with pull-down resistor.
2016-05-08 4:27 AM
I have seen a code where a GPIO pin is configured as output in push-pull mode but the pin is driven by an external circuit to low some times
Where? Provide some context. Is it a bus interface where the direction might be reconfigured? Clearly creating this kind of contention is not desirable.2016-05-09 12:45 AM
I/O ports are being used as data bus. Port bits are connected to LCD. After going through the code I realized that no read is being done, so I guess it is ok to have push-pull. Ideally open collector with pull-ups, but speed may be hampered. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.