cancel
Showing results for 
Search instead for 
Did you mean: 

Query about STM32F2

aamirali641989
Associate II
Posted on October 08, 2013 at 13:58

1. What is the purpose of internal regulator, to what it provides voltage - to core?

What does pin vcap1 & vcap2 has to do with it. I read that 0.1uf or 2.2uf cap to connected depending on regulstor used or not.

2. In microxplorer, it shows to mcu with STM32F205. One is STM32F205RxTx(RevAZB) & other is STM32F205RxTx.

What does RevAZB means here

3. For NXP there is Armwizard (http://alexan.edaboard.eu/index.php?page=armwizard)

to configure its peropheral also. Is there any such tool for STM32F205 also. Microxplorer configure only pins

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 08, 2013 at 14:09

1) Provides 1.25V to the core

2) Stepping/Revision of silicon die being used

3) Don't think so, they also create an ignorance of the detail.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..