cancel
Showing results for 
Search instead for 
Did you mean: 

Quadrature Encoder Channels

mattfox
Associate II
Posted on August 09, 2013 at 20:11

I'm working with the STM32F3 Discovery board.  I'm wondering if it is possible to use a timer in encoder interface mode with the signals coming in on Channels 1 and 4.  Do you have to use channels 1 and 2?  Does the Timer just measure the difference between the two channels that are initialized?  Thanks for the help in advance!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mattfox
Associate II
Posted on August 09, 2013 at 21:00

I've solved my problem, even if I'm not too sure of the answer to this question.  I don't think that it's possible from what I read online, but I figured out a way to use channels 1 and 2 on a different bus for my implementation.

Posted on August 12, 2013 at 01:11

Typically it pairs TI1 and TI2 for the encoder, I'm not sure you can use it with other pairings like 3/4.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..