cancel
Showing results for 
Search instead for 
Did you mean: 

PWM for stepper motor

feres_cherif
Associate II
Posted on April 24, 2013 at 11:05

Hi all,

plz i need to generate a signal like this one to control a stepper motor: 0690X00000603GGQAY.jpg

if you have an idea don't hesitate plz. I found an example named ''6 steps'' which contains a signal like this one but it doesn't work
1 REPLY 1
crt2
Associate II
Posted on April 24, 2013 at 16:49

It doesnt work could mean also that you need to power your motor and/or Cortex? Idea? Take 2 PWM lines and set the signals. You can even make it manually with timers if you feel hardcore.