cancel
Showing results for 
Search instead for 
Did you mean: 

provide design files(layout( of X-NUCLEO-IDW01M1

chaitanya jasti
Associate II
Posted on February 24, 2017 at 14:10

We need layout files of X-NUCLEO-IDW01M1

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on February 25, 2017 at 14:19

The Gerber format is an open ASCII vector format for 2D binary images. It is the de facto standard used by printed circuit board (PCB) industry software to describe the printed circuit board images: copper layers, solder mask, legend, etc.

View solution in original post

6 REPLIES 6
Amel NASRI
ST Employee
Posted on February 24, 2017 at 14:31

Please refer to

http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-connect-hw/x-nucleo-idw01m1.html

 on ST web site.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

john doe
Lead
Posted on February 24, 2017 at 14:32

http://www.st.com/en/ecosystems/x-nucleo-idw01m1.html

Gerber files, schematic, and BOM are there if you scroll down

Posted on February 25, 2017 at 06:49

Can we get the layout file

On Fri, Feb 24, 2017 at 7:03 PM, john doe <st-microelectronics@jiveon.com>

Posted on February 25, 2017 at 14:19

The Gerber format is an open ASCII vector format for 2D binary images. It is the de facto standard used by printed circuit board (PCB) industry software to describe the printed circuit board images: copper layers, solder mask, legend, etc.

Posted on February 27, 2017 at 12:07

Ok,

We are using

STM32L152RET6

How to set up RTC.Is there any internal RTC?

On Sat, Feb 25, 2017 at 6:50 PM, john doe <st-microelectronics@jiveon.com>

Posted on February 28, 2017 at 14:14

Hello,

If the subject change, I suggest you to open a new discussion thread.

This will ease any research.

Kind regards

Sirma