cancel
Showing results for 
Search instead for 
Did you mean: 

Programing FLASH in a STM32G030C8T6 throubles

woutnme
Associate II

Debuging the function when try this

HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, (uint32_t) 0x08001000, DATA_64)

get in FLAH->SR = 8, its the PROGERR bit, i unlock the flash before, below part of code

HAL_FLASH_Unlock();

 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, (uint32_t) 0x08001000, DATA_64) == HAL_OK)

 {

 HAL_GPIO_WritePin(Y0_GPIO_Port, Y0_Pin, GPIO_PIN_SET);

 }else{

 HAL_GPIO_WritePin(Y2_GPIO_Port, Y2_Pin, GPIO_PIN_SET);

 }

 HAL_FLASH_Lock();

Debuging it can see the PROGERR sets after 2nd word write...

 static void FLASH_Program_DoubleWord(uint32_t Address, uint64_t Data)

{

 /* Set PG bit */

 SET_BIT(FLASH->CR, FLASH_CR_PG);

 /* Program first word */

 *(uint32_t *)Address = (uint32_t)Data;

 /* Barrier to ensure programming is performed in 2 steps, in right order

  (independently of compiler optimization behavior) */

 __ISB();

 /* Program second word */

 *(uint32_t *)(Address + 4U) = (uint32_t)(Data >> 32U);

}// AFTER THIS THE PROGERR IS SET

Add, i try configure the LATENCY to 2 but no effects.... same error

Bit 3 PROGERR: Programming error Set by hardware when a double-word address to be programmed contains a value different from '0xFFFF FFFF' before programming, except if the data to write is '0x0000 0000'. Cleared by writing 1.

The address pass the assert_param(IS_FLASH_PROGRAM_ADDRESS(Address)); correctly

and use the 0x08001000 its 2nd page of memory. I dont find the problem anywere....

Thanks for hepl in advance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
woutnme
Associate II

Im checking the code the data memory and is right cant write because not have FFFFFFFF in the memory before, but if i want change only one value of 64bit in the page i will need read all page to rewrite with the same data only the data changed modified??? that its the correct way? i will store holding registers from MODBUS.....