cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with USB Macrocell on STM32F103

brianwood9
Associate
Posted on April 06, 2009 at 13:37

Problem with USB Macrocell on STM32F103

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
brianwood9
Associate
Posted on May 17, 2011 at 13:08

I have an application that runs on a STM32F103 which is essentially a USB virtual COM port for Windows. It adheres to the USB Communication Device Class Abstract Control Model standard. I am running into a problem with Bulk OUT transactions; my endpoint packet size is set to 64 bytes. If the overall transfer is greater than 64 bytes, intermittently one of the maximum size (64 byte) packets will generate the normal Correct Transfer Received interupt but when I read the number of bytes using the GetEPRxCount() from ST’s USB library it reports 63 bytes. I have a USB protocol analyzer so I know all the bytes are sent by the host (Windows). No errors are reported in the interrupt status register, and all 64 bytes are there if I force a 64 byte read in this situation.

Has anyone else encountered this problem ?