cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Uppercase filename in STM32CubeExpansion_SUBG1_V1.0.0

Uwe Bonnes
Chief
Posted on February 29, 2016 at 18:27

Hello,

the file listed below still contain mixed case include file name:

/Drivers/BSP/STM32L0xx_Nucleo/stm32l0xx_nucleo.c:#include ''STM32l0xx_nucleo.h''

./Drivers/STM32L0xx_HAL_Driver/Inc/stm32l0xx_hal_rcc.h:#include ''stm32L0xx_hal_rcc_ex.h''

This results in errors when compiling the P2P example for Nucleo-L053 with SW4STM32 on Linux.

Please correct
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 08, 2016 at 10:55

Hi bonnes.uwe,

Thanks for bringing this issue to our attention.

Please note that it is planned to align  STM32CubeExpansion_SUBG1 with HAL drivers available in last STM32CubeL0 package. 

So, the reported bug will be fixed in the new version coming soon.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.