cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with FMC_NOR Sample Program.

Rohit  Mishra
Associate II
Posted on September 04, 2017 at 07:45

I am working on STM32F756-EVAL2 Board, and wanted to use NOR Flash Memory to Store some configuration data. But i am facing some problem. I am not able to write any thing into NOR memory.(But able to perform read Operation).

I also checked with the sample program of FMC_NOR provided for the evaluation board. 

The program provided below Writes a buffer to Nor Flash and then reads it , compares with the written data. Till here the program works fine.

Now in the same example when i perform only read operation to read previously stored data, it is read as blank. 

What could be the issue...... 

int main(void)

{

/* Enable the CPU Cache */

CPU_CACHE_Enable();

HAL_Init();

SystemClock_Config();

/* Configure LED1 and LED3 */

BSP_LED_Init(LED1);

BSP_LED_Init(LED3);

/*♯♯-1- Configure the NOR device ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

/* NOR device configuration */

hnor.Instance = FMC_NORSRAM_DEVICE;

hnor.Extended = FMC_NORSRAM_EXTENDED_DEVICE;

NOR_Timing.AddressSetupTime = 4;

NOR_Timing.AddressHoldTime = 3;

NOR_Timing.DataSetupTime = 8;

NOR_Timing.BusTurnAroundDuration = 1;

NOR_Timing.CLKDivision = 2;

NOR_Timing.DataLatency = 2;

NOR_Timing.AccessMode = FMC_ACCESS_MODE_A;

hnor.Init.NSBank = FMC_NORSRAM_BANK1;

hnor.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;

hnor.Init.MemoryType = FMC_MEMORY_TYPE_NOR;

hnor.Init.MemoryDataWidth = NOR_MEMORY_WIDTH;

hnor.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;

hnor.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;

hnor.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;

hnor.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;

hnor.Init.WaitSignal = FMC_WAIT_SIGNAL_ENABLE;

hnor.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;

hnor.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE;

hnor.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;

hnor.Init.ContinuousClock = NOR_CONTINUOUS_CLOCK;

/* Initialize the NOR controller */

if(HAL_NOR_Init(&hnor, &NOR_Timing, &NOR_Timing) != HAL_OK)

{

   /* Initialization Error */

   Error_Handler();

}

// /*♯♯-2- NOR memory read/write access ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

// /* Fill the buffer to write */

// Fill_Buffer(aTxBuffer, BUFFER_SIZE, 0xD20F);

//

// /* Write data to the NOR memory */

// for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++)

// {

// /* Write data to NOR */

// HAL_NOR_Program(&hnor, (uint32_t *)(NOR_BANK_ADDR + WRITE_READ_ADDR + 2*uwIndex), &aTxBuffer[uwIndex]);

//

// /* Read NOR device status */

// if(HAL_NOR_GetStatus(&hnor, NOR_BANK_ADDR, PROGRAM_TIMEOUT) != HAL_NOR_STATUS_SUCCESS)

// {

// return HAL_NOR_STATUS_ERROR;

// }

// }

/* Read back data from the NOR memory */

if(HAL_NOR_ReadBuffer(&hnor, NOR_BANK_ADDR + WRITE_READ_ADDR, &aRxBuffer[0], BUFFER_SIZE) != HAL_OK)

{

return HAL_ERROR;

}

/*♯♯-3- Checking data integrity ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

uwWriteReadStatus = Buffercmp(aTxBuffer, aRxBuffer, BUFFER_SIZE);

if (uwWriteReadStatus != PASSED)

{

/* KO */

/* Toggle LED3 */

while(1)

{

BSP_LED_Toggle(LED3);

}

}

else

{

/* OK */

/* Turn on LED1 */

BSP_LED_On(LED1);

}

   /* Infinite loop */

   while (1)

   {

   }

}

#flash-writing
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0