Skip to main content
dnm_es
Associate
January 12, 2015
Question

Problem with DAC stm32f103rd

  • January 12, 2015
  • 2 replies
  • 606 views
Posted on January 12, 2015 at 18:29

Hello, I would like generate two different signal with the channel 1 and 2 of DAC. I've used two different timer (TIM6 and TIM2) and one DMA address (DAC_DHR12RD_Address    0x40007420). I can generate the signals separate but I try to generate the together (each signal with different DAC) It don't work.

Any ideas??

Thank you

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 12, 2015
    Posted on January 12, 2015 at 18:59

    Any ideas??

    Like pointing each DMA to the appropriate DAC register?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    dnm_es
    dnm_esAuthor
    Associate
    January 13, 2015
    Posted on January 13, 2015 at 08:51

    This is my code. I generate one signal with DAC1, this is works, but when I try to generate the signal with DAC2 this is works and the signal of DAC1 stops workings

    #define         DAC_DHR12R1_Adress             0x40007408

    #define         DAC_DHR12R2_Adress             0x40007414

    const           uint8_t                 Escalator8bit[2] = {0x0, 0xFF};

    void DMA_Setup(int dec_channel, int8_t DMA_Class, )

    {

          DMA_Channel_TypeDef* DMA_Channel;

              

              DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;                             /* DMA operation mode */

              DMA_InitStructure.DMA_Priority = DMA_Priority_High;                         /* Specifies the priority for the DMA Channel */

              DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;                                /* Specifies if the DMAy Channelx will be used in memory-to-memory transfer */

              DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;            /* Specifies whether the Peripheral address register is incremented or not */

              DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

     

                  if(dec_channel==0)                                                      /* If dec_channel=0 I use DAC1 */

                  {

                        DMA_InitStructure.DMA_PeripheralBaseAddr = DAC_DHR12R1_Adress;

                DMA_Channel=DMA2_Channel3;    

                  }

                  else

                  {

                        DMA_InitStructure.DMA_PeripheralBaseAddr = DAC_DHR12R2_Adress;

                DMA_Channel=DMA2_Channel4;

                  }

     

              DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&Escalator8bit;

              DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST;

              DMA_InitStructure.DMA_BufferSize = 2;

              DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

              DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

          DMA_DeInit(DMA_Channel);               

              DMA_Init(DMA_Channel, &DMA_InitStructure);

              

                 /* Enable Channely for DMAx */

              DMA_Cmd(DMA_Channel, ENABLE);

     

    }