2017-10-23 4:12 PM
Hello everybody,
I am new here and i'm just using a STM32F411RE, as a hobby today, but I have encountered a problem with compilation of my binary file. It is just not working and I am trying to figure it out for many days now so I'm hoping that you will give me some advice !
I have the following code, just to light up the led user in order to understand the process of registers, clocks, interrupts etc...
https://os.mbed.com/compiler/&sharpnav:/Essai_Led/stm32;
&sharpinclude 'stm32f4xx.h'
&sharpinclude 'system_stm32f4xx.h' void SystemInit(void) ; /* Initialization of the system with this file */int main() {
/* Configuration en sortie push pull de la pin 1 */
RCC->AHB1ENR = RCC->AHB1ENR | 0x00000001 ; /* Autorisation de l'horloge des p�riph�riques */ GPIOA->MODER = GPIOA->MODER | 0x00000400 ; /* mise � 01 des bits en outpout du port LED (1 ici ) */ GPIOA->OTYPER = GPIOA->OTYPER | 0xFFFFFFBF ; /* mise � 0 du bit du registre pour output push pull */ /* Configuration du timer */ RCC->APB1ENR = RCC->APB1ENR | 0x00000001 ; /* Enable clock TIM2 */ TIM2->ARR = 3332 ; TIM2->PSC = 7199 ; TIM2->DIER = TIM2->DIER | 0x0001 ; /* Autorisation interruption du timer */ /* Autorisation interruption */ RCC->CIR = RCC->CIR | 0x00000F00 ; /* Autorisation interruption en fonction de l'horloge*/ NVIC->ISER[0] = NVIC->ISER[0] | (1 << 28); /* activation de l'interruption 28 */ NVIC->IP[28] = NVIC->IP[28] | (1 << 4); /* Priorit� (1) */ /* Lancement du timer */ TIM2->CR1 = TIM2->CR1 | 0x0001 ; /* Debordement Timer */ while(1) { } }void TIM2_IRQHandler(void){
TIM2->SR = TIM2->SR & 0xFFFE ; /* Remise � 0 du bit UIF */ /* Allumage LED toutes les secondes */ /* Allumage/ETEINT LED */ GPIOA->ODR = GPIOA->ODR ^ (1 << 5);}
Have you got some remarks about it ? why my code does not work when I flash it in my MCU ?
Thanks a lot,
Charley
#incomplete-code