cancel
Showing results for 
Search instead for 
Did you mean: 

Problem CAN Stm32f107RCT6 v2 to v3

ruiserra
Associate
Posted on July 02, 2010 at 01:17

Hello,

I have problems in configuring the CAN on STM32F107RCT6 with version 3.0 in this post i am sending the code for version 2 that i have working and sending the code for version 3.0 that doesen't work.

I have already examined the output of CAN_TX before the CAN transceiver, and note that the data to be transmitted is not at the correct frequency. In my opinion the problem should be in the configuration of the crystal in the micro RCC configuration, but i already tryed to solve this but so far notting.

The crystal I want to use is the external crystal from 12MHz.

Thanks for your time.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0