Skip to main content
jean_prieur
Associate III
June 8, 2015
Question

Powf (power exponent) don't return float values

  • June 8, 2015
  • 13 replies
  • 2899 views
Posted on June 08, 2015 at 13:03

Hi everybody,

I use the function powf (that is supposed to return a float), included in the library

#include <math.h>

This is the definition of the function in math.h :

float
powf _PARAMS((
float
, 
float
));

When I run this code:

float
EXPONENT_BASE_2;
EXPONENT_BASE_2 = powl(4.73, 0);

The result is

125410439

instead of

1254104217423

Powf don't return a float but a int. Do you have any idea of what happens? i also tried pow and powl but it's the same result...Thanks a lot!

    This topic has been closed for replies.

    13 replies

    AvaTar
    Senior III
    June 8, 2015
    Posted on June 08, 2015 at 13:21

    This is the definition of the function in math.h :

    float
    powf _PARAMS((
    float
    , 
    float
    ));

    When I run this code:

    float
    EXPONENT_BASE_2;

    EXPONENT_BASE_2 = powl(4.73, 0);

    Perhaps you should use a different character font in your editor, otherwise you would realized that you call the wrong function. No wonder the function returns an integral number. Edit:

    The result is

    125410439

    instead of

    1254104217423

    BTW, I would not expect such a numerical resolution from a float variable ...
    Tesla DeLorean
    Guru
    June 8, 2015
    Posted on June 08, 2015 at 15:00

    And this is with what tool chain, and printed out how?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jean_prieur
    Associate III
    June 8, 2015
    Posted on June 08, 2015 at 15:14

    I use GNU Tools ARM Embedded 4.9 and I print out the variable on my board graphic screen, or with the debugger of Coocox.

    About the example I give, it's just to illustrate my problem: I have only int returns, even when it's supposed to returns a floats.

    AvaTar
    Senior III
    June 8, 2015
    Posted on June 08, 2015 at 16:04

    I have only int returns, even when it's supposed to returns a floats.

     

    No.

    If your code is exactly like the example you give, it is not.

    The powl() function returns a long (integer) value - casting to float doesn't make it a float.

    Tesla DeLorean
    Guru
    June 8, 2015
    Posted on June 08, 2015 at 18:07

    Do you have any idea of what happens?

    24-bit mantissa? So perhaps 7-8 digits?
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jean_prieur
    Associate III
    June 9, 2015
    Posted on June 09, 2015 at 09:24

    Sorry but I didn't understand... The function powf is supposed to return floats... Otherwise why do they created pow (to return an int) and powf (to return a float) ? A power exponent without floating point is quite useless in my case...

    Thanks!

    AvaTar
    Senior III
    June 9, 2015
    Posted on June 09, 2015 at 12:45

    Sorry but I didn't understand... The function powf is supposed to return floats...

     

    To be more blunt: you are calling the wrong function in your given example.

    The pow

    F

    () function returns a float value, but the pow

    L

    () function (

    which you actually called

    ) does return an integer. (Capitalisations in function names only for clarification).

    Tesla DeLorean
    Guru
    June 9, 2015
    Posted on June 09, 2015 at 14:47

    Sorry but I didn't understand... The function powf is supposed to return floats... Otherwise why do they created pow (to return an int) and powf (to return a float) ? A power exponent without floating point is quite useless in my case..

    Then you really need to review your understanding of floating point, and precision, and then pick appropriately sized variables to hold the digits you expect.

    You have a 32-bit float, holding a 24-bit mantissa (the digits), and 8-bit exponent.

    In 24-bit unsigned numbers you have a range of 16 million, 16777216, observe that it has 8 digits with values, if you multiply it by an exponent, say 6 (106), you have 16777216000000, you DON'T get any more significant digits, you get ZEROS. The processor uses base 2 (binary) exponents, but the concept is the same, except some fractions/numbers are going to be poorly represented. You're not going to magically get 16 digits of precision you seem to be expecting.

    If you're using floating point it's critical you understand how they work and their limitations.

    http://en.wikipedia.org/wiki/Single-precision_floating-point_format

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    June 9, 2015
    Posted on June 09, 2015 at 15:05

    Capitalisations in function names only for clarification

    OP : ''Powf don't return a float but a int. Do you have any idea of what happens? i also tried pow and powl but it's the same result.''

    Stop banging on about F or L, it's not the underlying issue here.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stm322399
    Senior
    June 10, 2015
    Posted on June 10, 2015 at 09:52

    Jean,

    show us the printf (or any vnsprintf powered function you used) format string used to display your float.

    To make sure that powf returned a float, you can print out your_float*1000.0, the non-null decimal part will prove that powf returned a float. Otherwise it will give a suspicion of powf to be buggy.