2022-01-19 3:39 PM
I use cubemx to generate clock config
And I use a flip pin and oscilloscope to check the speed.
here is what i did
clock setting
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 40; //160MHz
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
/** Initializes the peripherals clocks
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2
|RCC_PERIPHCLK_I2C3|RCC_PERIPHCLK_USB;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.I2c3ClockSelection = RCC_I2C3CLKSOURCE_PCLK1;
PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}in the main function
I use a flip to check the waveform
//testing
while(1)
{
FlipBlueLED();
TM_DelayMillis(2);
}
void TM_DelayMillis(uint32_t millis) {
/* Multiply millis with multipler */
/* Substract 10 */
millis = 1000 * millis * multiplier - 10;
/* 4 cycles for one loop */
while (millis--);
}Suppose it shall be 2ms waveform, but it is 9ms waveform (period is 18ms)
So it is about 4.5times slower.
Even I change the PLL setting, it doesn't gets faster..
Anyone, please help.
2022-01-19 5:11 PM
What is HSE frequency? 40Mhz seems high. What is multiplier?
Your mistake is likely assuming the loop takes exactly 4 ticks as well as using a loop which can be optimized out.
Use a hardware based time rather than a software loop subject to the whims of the compiler.
2022-01-20 1:49 AM
To check the frequency with an oscilloscope you have to use the MCO output.
2022-01-20 2:13 PM
I didn't see MCO output in cubemx. I am using stm32G431
which pin is used for this purpose.
2022-01-20 2:13 PM
8MHz
2022-01-20 2:24 PM
Hello
Thanks for your reply
I tried again from scratch using cubemx to generate a new project.
Also I use a PWM to get the pulse. Starting from brand new project with cubemx.The clock is shows as what supposed to be.
And then I copied the code from old project to new project section by section, now it looks everything is working well. I checked the pin for LED with oscilloscope, the frequency is correct.
Really don't know what is going on.
Using cubemx to generate a brand new project and start from scratch, it is an easy way to test.