cancel
Showing results for 
Search instead for 
Did you mean: 

Parametric search - HSE available or not

soren
Associate II
Posted on February 07, 2016 at 21:33

Hi, I have tried in STM32Cube and I have tried the online parametric search. I want to filter the STM32L0xxx parts so I only get those which have external HSE clock connections available. This ought to be possible, have I overlooked something? It is usually one of the first criteria that comes up in a design - is crystal precision and stability needed, or is it not..

Thanks for any input on how to do that.

Regards, Soren
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 07, 2016 at 21:37

Pretty sure they all provide for one, CAN and USB normally requiring the accuracy afforded by them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
soren
Associate II
Posted on February 09, 2016 at 12:27

Hi Clive, thank you

Many L0 devices don't have a HSE. For example, STM32L052 in the UFQFPN32 package don't have any OSC pins. They do have a 1% or something HSI which is good enough for CAN and USB. However, I need better than that...

Regards

Soren