cancel
Showing results for 
Search instead for 
Did you mean: 

OTG_FS_DAINT RO or RW ?

dimax
Senior
Posted on March 14, 2013 at 15:30

Is OTG_FS_DAINT register ReadOnly or Read/Write ?

According to the reference it is RO but in USB Demo source code provided by ST I see many writes to this register of 0xFFFFFFFF in attempt to clear pending INT bits.

Who is wrong FW or Manual?

I think FW as manual clearly states ''Bits in this register are set and cleared when the

application sets and clears bits in the corresponding Device Endpoint-x interrupt register

(OTG_FS_DIEPINTx/OTG_FS_DOEPINTx).''.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0