2022-01-18 2:16 AM
Hello, i am trying to communicate with an MRAM memory (Micron) via octoSPI but i can't manage to make it work! i already looked at the ST code examples and i got the same configuration as the examples but it just doesn't work. Please help!
PS: i am using OSPI1 on a Flash memory and the OSPI2 on my MRAM.
You will find my code bellow:
MX_OCTOSPI2_Init(void)
static void MX_OCTOSPI2_Init(void)
{
/* USER CODE BEGIN OCTOSPI2_Init 0 */
/* USER CODE END OCTOSPI2_Init 0 */
OSPIM_CfgTypeDef sOspiManagerCfg = {0};
HAL_OSPI_DLYB_CfgTypeDef HAL_OSPI_DLYB_Cfg_Struct = {0};
/* USER CODE BEGIN OCTOSPI2_Init 1 */
/* USER CODE END OCTOSPI2_Init 1 */
/* OCTOSPI2 parameter configuration*/
hospi2.Instance = OCTOSPI2;
hospi2.Init.FifoThreshold = 1;
hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_MICRON;
hospi2.Init.DeviceSize = 32;
hospi2.Init.ChipSelectHighTime = 1;
hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi2.Init.ClockPrescaler = 1;
hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi2.Init.ChipSelectBoundary = 1;
hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;
hospi2.Init.MaxTran = 0;
hospi2.Init.Refresh = 0;
if (HAL_OSPI_Init(&hospi2) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.NCSPort = 2;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
sOspiManagerCfg.Req2AckTime = 1;
if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
HAL_OSPI_DLYB_Cfg_Struct.Units = 0;
HAL_OSPI_DLYB_Cfg_Struct.PhaseSel = 0;
if (HAL_OSPI_DLYB_SetConfig(&hospi2, &HAL_OSPI_DLYB_Cfg_Struct) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI2_Init 2 */
/* USER CODE END OCTOSPI2_Init 2 */
}ENABLE write command and write the buffer:
uint32_t NVRAM_WriteReg(OSPI_HandleTypeDef *hospi2, uint8_t *Value, OSPI_RegularCmdTypeDef sCommand)
{
/* Initialize the write register command */
sCommand.AddressMode = HAL_OSPI_ADDRESS_NONE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_8_BITS;
sCommand.Address = 0;
sCommand.AlternateBytes = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesMode = 0;
sCommand.AlternateBytesSize = 0;
sCommand.Instruction = 0x06;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.DataMode = HAL_OSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.NbData = 0;
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
// Configure the command
if (HAL_OSPI_Command(hospi2, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return HAL_ERROR;
}
/* Initialize the write register command */
sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
sCommand.AddressSize = HAL_OSPI_ADDRESS_8_BITS;
sCommand.Address = 0;
sCommand.AlternateBytes = HAL_OSPI_ALTERNATE_BYTES_NONE;
sCommand.AlternateBytesMode = 0;
sCommand.AlternateBytesSize = 0;
sCommand.Instruction = 0x87;//0x01;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
sCommand.DummyCycles = 0;
sCommand.NbData = 10;
sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytesDtrMode = HAL_OSPI_ALTERNATE_BYTES_DTR_DISABLE;
sCommand.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
if (HAL_OSPI_Command(hospi2, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return HAL_ERROR;
}
/* Transmission of the data */
if (HAL_OSPI_Transmit(hospi2, (uint8_t *)(Value), HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return HAL_ERROR;
}
return HAL_OK;
}HAL_OSPI_MspInit:
void HAL_OSPI_MspInit(OSPI_HandleTypeDef* hospi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(hospi->Instance==OCTOSPI1)
{
/* USER CODE BEGIN OCTOSPI1_MspInit 0 */
/* USER CODE END OCTOSPI1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_OSPI1_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/**OCTOSPI1 GPIO Configuration
PB0 ------> OCTOSPIM_P1_IO1
PB1 ------> OCTOSPIM_P1_IO0
PE10 ------> OCTOSPIM_P1_CLK
PE11 ------> OCTOSPIM_P1_NCS
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI1;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* USER CODE BEGIN OCTOSPI1_MspInit 1 */
/* USER CODE END OCTOSPI1_MspInit 1 */
}
else if(hospi->Instance==OCTOSPI2)
{
/* USER CODE BEGIN OCTOSPI2_MspInit 0 */
/* USER CODE END OCTOSPI2_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_OSPI;
PeriphClkInit.OspiClockSelection = RCC_OSPICLKSOURCE_SYSCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* Peripheral clock enable */
__HAL_RCC_OSPI2_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
/**OCTOSPI2 GPIO Configuration
PD3 ------> OCTOSPIM_P2_NCS
*/
GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF10_OCTOSPI2;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
HAL_GPIO_WritePin( NVSRAM_WP_GPIO_Port, NVSRAM_WP_Pin, ( GPIO_PinState )( 1 ) );
HAL_GPIO_WritePin( GPIOE, GPIO_PIN_11, ( GPIO_PinState )( 1 ) ); // CS FLASH
HAL_GPIO_WritePin( GPIOD, GPIO_PIN_3, ( GPIO_PinState )( 0 ) ); // CS NVRAM
//HAL_GPIO_WritePin( GPIOB, GPIO_PIN_0, ( GPIO_PinState )( 0 ) ); // SO1
/* OCTOSPI2 interrupt Init */
HAL_NVIC_SetPriority(OCTOSPI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(OCTOSPI2_IRQn);
/* USER CODE BEGIN OCTOSPI2_MspInit 1 */
/* USER CODE END OCTOSPI2_MspInit 1 */
}
}
2022-02-11 3:21 AM
Hello @SGUIG.1,
Can you please specify the board and the memory you are using?
Chahinez.
2022-02-11 4:15 AM
Not sure, but only the first instance initializes any pins, and then only two data pins.
Can you bring up both chips and probe the READ IDs?