NVIC_SystemReset not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 4:51 AM
I'm using the X-CUBE-SBSFU bootloader on a ST STM32G474VE.
Sometimes NVIC_SystemReset is not resetting the controller, only a power reset helps. Any ideas? The string "Image correctly downloaded" i can see everytime!
/* System Reboot*/
printf(" -- Image correctly downloaded - reboot\r\n\n");
HAL_Delay(1000U);
NVIC_SystemReset();
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 6:18 AM
@Community member I think the Option bytes was the solution, I changed them with the STM32 Cube Programmer the NRST Mode to 2, now its working and I can use PG10 as Push/Pull output
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:00 AM
What you describe sounds like a latch-up issue.
If you drive NRST externally, with a push-pull driver, this can prevent the core from resetting.
ST, in more recent parts, has decided to have NRST not completely reset them. Several of the protection methods require a power-on-reset actually occur, otherwise system loader code will run, rather than your code in FLASH
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:02 AM
Hi Clive
But it works like 70-80% of the updates...
Is there a precompiler setting or something to check? I'm using IAR.
Thaks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:03 AM
printf(" -- Image correctly downloaded - reboot\r\n\n");
HAL_Delay(1000U);
NVIC_SystemReset();
printf(" -- I'm not dead!!\r\n\n"); // If something is output, the mechanics of the pin are being interfered with
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:04 AM
PG10I'm using as an output
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:20 AM
Well I suppose that could complicate things. Not sufficiently read into the G4's to know the potential consequences of doing that.
You'd perhaps want to find a FAE to talk too, or file a Online Support Request to see if there is any gotchas. @Amel NASRI @Imen DAHMEN
Check also errata
You might try configuring the pin as an INPUT + PULL-UP prior to the NVIC_SystemReset()
>>But it works like 70-80% of the updates... Is there a precompiler setting or something to check? I'm using IAR.
Not sure it is something resolvable with a compiler setting
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:51 AM
@Amel NASRI @Imen DAHMEN @Tilen MAJERLE
Do you have an idea about this topic? Can I use the NRST PG10 PIN as Output or not? In cubeMX I can set it as push-pull, hope this is no bug in the MX?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 5:55 AM
Try reconfiguring the pin right before use here, it will indicate if it is a HW level issue, or something else.
Probing via USART1 might tell you if it is in the System Loader ROM.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 6:03 AM
I saw this entry, Its not working correctly but I saw when I connect with multi meter to measure the voltage level on this PIN the Core is getting resetted even if the impedance is really high...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-13 6:18 AM
@Community member I think the Option bytes was the solution, I changed them with the STM32 Cube Programmer the NRST Mode to 2, now its working and I can use PG10 as Push/Pull output