cancel
Showing results for 
Search instead for 
Did you mean: 

NVIC_SCBDeInit is in contraddiction with Cortex manual (??)

sirpak
Associate II

At the end of NVIC_SCBDeInit I see these instructions:

[...]

SCB->CFSR = 0xFFFFFFFF;

SCB->HFSR = 0xFFFFFFFF;

SCB->DFSR = 0xFFFFFFFF;

The first one is a status register. Why writing it?

For the second one the manual states:

"This register is read, write to clear. This means that bits in the register read normally, but writing 1 to any bit clears that bit to 0"

... "DEBUGEVT Reserved for Debug use. When writing to the register you must write 0 to this bit, otherwise behavior is Unpredictable."

The third one, DFSR does not exist in Cortex manual....

I am using STM32F103 and Cortex™-M3 Devices - Generic user manual

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0