2020-12-01 7:39 AM
I have configured my stm32g031 mcu as an i2c slave. My PC terminal is my master device and is connected to mcu via FTDI cable. When I do a i2c write, I can see mcu receives the data. But when I do an i2c read, I can see it reads 255 on my pc terminal.
When I debug my code, I can see the control coming to ,
uint8_t id = 0xA0;
HAL_I2C_Slave_Seq_Transmit_IT(&hi2c1, &id, 1, I2C_LAST_FRAME);But the mcu does not sends data out.
Below is the python code I use to communicate with MCU,
# Instantiate an I2C controller
i2c = I2cController()
# Configure the first interface (IF/1) of the FTDI device as an I2C master
i2c.configure('ftdi://ftdi:2232h/1')
# Get a port to an I2C slave device
slave = i2c.get_port(0x30)
#Write data
slave.write(b'\xAA')
#Read data
slave.read(1)Any suggestions what could be wrong here?
2020-12-04 2:40 PM
Whats your complete I2C slave code?
2020-12-04 4:44 PM
@KnarfB In main function I enable the Listen mode and then use the AddrCallback to receive or transmit data, as below
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c,
uint8_t TransferDirection,
uint16_t AddrMatchCode)
{
if(hi2c->Instance == I2C1)
{
uint8_t id = 0xA0;
if(TransferDirection == I2C_DIRECTION_TRANSMIT)
HAL_I2C_Slave_Seq_Receive_IT(&hi2c1, data, sizeof(data),I2C_FIRST_FRAME);
else
HAL_I2C_Slave_Seq_Transmit_IT(&hi2c1, &id, 1, I2C_LAST_FRAME);
}
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_I2C1_Init();
while(1) {
HAL_I2C_EnableListen_IT(&hi2c1);
}
}