cancel
Showing results for 
Search instead for 
Did you mean: 

Need extra UART, can the bxCAN peripheral be used?

mvonahnen
Associate III
Posted on July 30, 2014 at 21:04

I have an application where I need a large number of UARTs.  Can the CAN bus interface be used as an extra UART?

#stm32-bxcan-usart
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 30, 2014 at 21:15

Can the CAN bus interface be used as an extra UART?

No
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..