cancel
Showing results for 
Search instead for 
Did you mean: 

multiple usb descriptors

kilian23
Associate
Posted on October 29, 2012 at 10:29

Hello

I want that my STM32 has two usb descriptors. For example: If I plugin my STM32 Microcontroller to a pc, the pc should

recognize

the STM32 as two USB Devices. (For example as Camera and as Microphone Device).

Is this possible?

best regards
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stforum.tormod9
Associate II
Posted on October 29, 2012 at 20:45

Yes, that would be a composite device. Like all USB devices it will have only one device descriptor, but the interfaces can belong to different classes and be controlled by different drivers on the host computer.