cancel
Showing results for 
Search instead for 
Did you mean: 

Minimal Pulse width for triggering an EXT-Interupt

andywild2
Associate III
Posted on February 02, 2015 at 18:28

Hello to all,

I am using an STM32F2xx with 120Mhz.

An external interupt is triggered with a rising edge of a GPIO-Pin.

I looked in the datasheet, but I could not find information about the minimum pulse width at the GPIO-Pin in such  case.

How does the edge detector in the STM32F2xx work?

Does it detect the edge only if the signal is stable for a certain amount of clock cycles after the edge?

Thanks for your help!

Andy
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on February 02, 2015 at 19:33

Well the pin is feed into a pin synchronizer to get it into the AHB's clock domain, and then I'd expect it to enter a chain of flip-flops which could then determine a state change.

An ST FAE might be able to provide you with a specific diagram or illustration, and timing requirements (setup, hold).

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andywild2
Associate III
Posted on February 02, 2015 at 20:44

Hello Clive,

thanks for the quick answer!

I was wrong: There is an entry in the datasheet (I/O AC charakteristics):

tEXTIpw = 10ns

But please who does the synchronizer work?

In a  previous thread you said: ''The inputs do have a resynchronizer on them which has nyquist sampling properties''

Is it a real flip-flop or sampling device?

Thanks a lot

Andy

Posted on February 02, 2015 at 21:47

I'd expect it to be a chain of at least three flip-flops.

https://filebox.ece.vt.edu/~athanas/4514/ledadoc/html/pol_cdc.html

8-10ns seems like the width I'd half expected, perhaps with a latency of the order 24-30ns

Nyquist works in the digital domain too, if you get the rates wrong you'll observed all kinds of aliasing and beat effects.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..