2013-04-14 1:06 PM
Hi everyone
I use STMF1 and STMF4 devices for some time now but I just started with STM32F0 devices (Discovery board) and I have a quite strange problem. I created a class called Pin that can initialize any GPIO pin and use it (read, on, off, toggle, etc). When I create an instance of it like this :Pin LED(GPIOC, GPIO_Pin_8);
everything is okay, but if I do this :Pin* LED;
... LED = new Pin(GPIOC, GPIO_Pin_8); I have a flash memory overflow of 30492 bytes. When I'm invoking the size command before and after creating an instance of Pin with the first method I have this :Invoking: ARM Sourcery Mac OS X GNU Print Size
arm-none-eabi-size --format=berkeley base.elf text data bss dec hex filename 4356 2132 1128 7616 1dc0 base.elf Invoking: ARM Sourcery Mac OS X GNU Print Size arm-none-eabi-size --format=berkeley base.elf text data bss dec hex filename 4380 2132 1128 7640 1dd8 base.elf Nothing extraordinary and I have still plenty of free space. I'm using Eclipse with the GCC ARM toolchain on Mac OS X. Does anyone have an idea about the origin of this problem?2013-06-14 1:13 PM
I found a solution for this problem.
the ''--specs=nano.specs'' argument has to be passed to the linker to enable newlib-nano. The memory overhead for the new operator is less than 800 Bytes. Tested with GNU ARM 4.7 Hope it can helps someoneWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.