2016-09-13 8:01 AM
Ok, Here is the situation as follows.
You know where you are required to program your MCU. Technically speaking, having the following memory locations:
0x20003200
0x20003202
.
.
.
and you need to assign the following characters to each memory locations.
0x20003200 ==> '|'
0x20003400 ==> 'f'
.
.
.
and you can easily use IAR or other IDEs to program it and get what you want.
However, I am not willing to use any IDEs to program this specific parts of the memory?
Having said that, I am not going to completely refrain from using the IDE. I would like to flash it and then rewrite the memory with an external source to meet my need.
Therefore, I would like to make a GUI to detect the micro type that I have on my board firstly, then picks the characters of my choice and write it into my MCU.
What tools should I use? What is most important thing that I should care of?
These are the questions that I need to cope with.
To give you a better picture of this here is should be ended up with.
Choose your characters: [=,t,:,|,@,♯]
Choose the memory locations: [0x20003200, 0x20003202, 0x20003204, 0x20003206, 0x20003208, 0x20003210]
Thank you in advance!
p.s. And please don't advise me to get Elprotronic in order to do this! With all do respect! :)
#memory #stm32f1072016-09-16 6:47 AM
2016-09-16 7:14 AM
The System Loader in ROM also permits connectivity via USART1, and provides a protocol to read/write memory. There are also MCU DBG DEVID registers which can be used to identify the STM32, Core, along with ROM based constants for RAM and FLASH.