2010-05-22 9:22 AM
Mass storage problem with USB
2011-05-17 4:52 AM
Hello, I have had a similar problem.. if you have a look at my SPI Problems post I have a driver that is compatible with this device. I think you mean that you are communicating with the device as an SPI device not USB.
To get data to be stored the key is to erase the page/sector before you write and also make sure that the Sector Protect bit is reset before you attempt any operation. Have you read the datasheet for the EEPROM device ? because that will tell you about write requirements.2011-05-17 4:52 AM
hi,
thanks for your answer first. But i was used M25P16 flash to my media for mass storage device. so when i was insert my device to the PC, the usb flow not run into scsi write 10 state and it can't format.2011-05-17 4:52 AM
hi,
I have attached two files and the code are modify by mass_mal files. Does there have to amend? thx