cancel
Showing results for 
Search instead for 
Did you mean: 

LTDC using internal SRAM, How much SRAM?

Asantos
Senior
Posted on February 10, 2017 at 21:40

Hi,

 I would like to use a 320x240 TFT RGB interface display using the STM32F767ZI internal SRAM. But I can't figure out what is the minimum SRAM required for the frame buffer. For 16 bits RGB565 would be 320x240x2 = 153600 bytes?  

 Ari.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
T J
Lead
Posted on February 10, 2017 at 22:10

Yes, I believe that is correct...

320x240 TFT with 16bit RGB565 would be 320x240x2 = 153,600 bytes

the next question is how much CPU horsepower is used to refresh the display continuously ?

does the processor temperature rise significantly running an LCD ?

are you using A/Ds ?  I wonder how the analog converters drift when the processor is under load..

This is why most solutions are using the SPI port but it suffers 1000x slower update